This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4490: About the default settings [Factory shipment values]

Part Number: AFE4490


Tool/software:

Is the default or factory value 0000?

Or is it the Reset Value = **** part of the datasheet? please tell me.

By the way, with the settings in the datasheet
If I accidentally write 1 in a place like the one where Bits D[23:17] Must be '0' is written as shown below,

the IC will only malfunction,

and if I rewrite the setting value in SPI, will it return to its original state?
Reason: I needed to know this because I needed to be able to write any number
into the AFE4490 settings via a microcontroller on a tablet or other device.