This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi TI,
In my custom board ADS8365 ADC is selected, but size is not feasible on my board.
So, Could you please suggest ADC part number which Simultaneous sampling ADC, Single ended more than 4-channel ADC.
Input Voltage Range : 0 - 5 V
Sampling rate : more than 250 KSPS
Resolution : More than 12 bit (preferred 14 or 16 bit)
Form Factor/Package : smallest (less than 6mm X 6 mm)
No of Analog inputs : 5 No of channel , Single-Ended
Hi Sanath,
The 6x6mm is going to be a potential problem, how does the ADS8363 look for you? There are 8 channels in total, but you can only sample 2 at a time. Next smallest option is the ADS7864 if you can deal with a parallel interface.