This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPL0401B-10: Adjusting PMIC FB resistor using digital potentiometer

Part Number: TPL0401B-10
Other Parts Discussed in Thread: LM61480,

Tool/software:

I am currently considering using the TPL0401B-10 to adjust the FB resistor of the LM61480 to achieve an output voltage range of 5V to 12V. The input voltage is 18V to 36V, and the output current is 5A. I would like to know if the TPL0401B-10 can meet these requirements."