Tool/software:
Dear TI Community,
I am currently working with the ADS1220 and facing some challenges with my configuration and data readings. Here are the details of my setup:
please do verify Schematic Diagram Two Wire RTD And please check my code .
Configuration:
- 
Register 0: Command 0x66- AINp = AIN1,AINn = AIN0
- Gain = 8
- PGA = Enabled
 
- 
Register 1: Command 0x04- Data Rate = 20 SPS
- Normal mode
- Continuous Conversion mode
 
- 
Register 2:command 0x55h 
- 
External Reference configuration(REFP0,REFN0) - Simultaneous 50Hz/60Hz rejection
- IDAC = 500 µA
 
- 
Register 3:command 0x80 
- 
IDAC1 connected to AIN3/REFN1 
Procedure:
- I first send the command 0x06(Reset Command).
- Before reading data, I send the command 0x08(Start Conversion).
Issue:
I am using a PT100 RTD for temperature measurement, but the ADC raw data does not change with varying temperatures. I am only receiving two values: 8388351 and 8387839, regardless of the temperature applied to the RTD.
Questions:
- Is this issue likely related to hardware or software configuration?
- Are there any specific settings or steps I might be missing that could help improve the consistency of the readings?
I appreciate any guidance or suggestions you can provide.
 
Thank You!