Other Parts Discussed in Thread: ADS1263
Tool/software:
Hi ,
I am using ADS1263EVM-PDK. I want to measure current using differential input, voltage across shunt resistor( 1 ohm) . used INA0 and INA1 .
i am using GUI tool. the full scale voltage is 5 v , taking internal reference voltage +2.5 v and -2.5 v. using gain 32, sinc5 filter , 38400 SPS.
i am getting below reading as compared to dmm 6500
| Shunt val = 1 ohm | ||
| Load Value | shunt current(uA)(ADC1) |
Dmm current(uA)
|
| 5.9 k | 874 | 834 |
| 12.48 k | 415 | 399 |
| 25 k | 205 | 201 |
| 50 k | 101 | 98 |
| 100 k | 44 | 49 |
| 200 k | 22 | 25 |
| 508 k | 8 | 9 |
| 1 m | 650nA | 4.9 |
we want measure current in range 1uA to 3A
you can see the current value is not matching to the dmm 6500
please help us to solve
Thanks ,
Tushar Gajjar