Part Number: DAC81401
Tool/software:
Hello,
I recently purchased the DAC81401 Evaluation Module. Unfortunately, when I attempted to power up the module, something went wrong. I had initially set the jumpers following the layout shown in “Figure 3-2. Default Header Settings with High Voltage Gain Stage Disabled” on page 11 of the datasheet. However, I didn’t realize that this configuration wasn’t intended for external biasing. It seems I may have made an error here.
When I powered the module under these settings, I noticed a current draw of around 70mA at both +5V and -5V for all biases, except the high-voltage one, which i didn't connect. After adjusting the jumpers correctly and connecting only the power supplies to DVDD (J6), AVDD (J3), and AVSS (J4)—each set to either +5V or -5V—the biasing current has now dropped to 1mA on both channels of the power supply. This current level seems somewhat low to me.
When I attempt to use the software to control the board, I’m not seeing any response from the board pins when changing the registers. I’m concerned that one of the chips may have been damaged in the process.
Any guidance or insights you could provide would be greatly appreciated.
Kind regards,
Thiemo