Part Number: ADC14L020
Tool/software:
I am very confused by the datasheet on how to calculate nominal digital code outputs from the ADC. Table 1 and Table 2 and Figure 2 leave a lot to be desired and do not give out specific examples which is helpful but also not that helpful. Can anyone give specific examples of codes being outputted? Ex: Vin+ set at this voltage and Vin- set at this voltage produces a code of 14'h0800.
Also do I have it right that the LSB is (2.6)/(2^14) = ~0.0001587V? I might be interpreting the data sheet wrong when it states full scale input voltage range. I assume that is 2.6V-0V.