Tool/software:
I have a question about how to start up the TSC2003.
When using the TSC2003, it is rare that the sensor value cannot be read correctly. Figure 1 shows the waveforms of SCL (yellow) and SDA (green) at this time. SDA is stuck low at the data area (red circle in the figure).
I assumed that the startup method was incorrect, so I took a software solution based on "Powering Up the TSC2003 Correctly" (toggle SCL 9 times or more after startup, then issue a start).
Figure 2 shows the waveforms at that time.
However, the symptoms of the TSC2003 do not improve. Are the above solutions correct? Are there any other possible causes?