This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS52J90: Auto offset mode: how is computed the dc value value substracted

Part Number: ADS52J90

Tool/software:

Hello

I'm willing to use the auto offset removal feature (chap 8.3.5.1.2) .

The DS doesn't specify how the DC is computed.

Is it computed in background all the time and might change over the time?

Or is it computed only once, after the TX_TRIG or the MANUAL_START has occured, using the number of samples specified in reg AUTO_OFFSET_REMOVAL_ACC_CYCLES?

In that case the DC value will stay the same for all the time of operation.

Regard,

Pierre

  • There are two options 

    1) If you know the offset already you can write that offset

    2) If you dont know offset , once tx_trig is given it will accumulate based on start sample (TXTrig or OFFSET_REMOVAL_START_MANUAL) and number of samples to accumulate (AUTO_OFFSET_REMOVAL_ACC_CYCLES). This happens on every tx_trig.

    Does this answer your query ?

  • Hi,

    Method 1) give good results but requires a manual action. Kind of calibration.

    Method 2) does not give good result in my application. This is the reason of my question. In my application, the system only generate one TX_TRIG for all the system operation time. It is generated at startup time.

    So if I clearly understand your answer, in my application, the DC offset will only be computed once and probably not at the best moment. Right?

  • Yes correct . You can readout the compute offset value and check whether it matches your offset expectation . 

    How do you know offset is from device or input ?Are you ac coupling the input ? 

  • Yes, the ADC is AC coupled.
    The worst offset value I have manually measured is 38 LSB offset. I guess , that matches the datasheet data of +/-7mV.

    I am looking at the OFFSET_REMOVAL_START_MANUAL of the auto offset correction mode. Maybe that's a better way to get the auto mode doing the job in my application.

  • Ok. You can use that .Hopefully with this you can get the required offset .