This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS127L21: Synchronizing multiple devices together

Part Number: ADS127L21


Tool/software:

Hey Folks! 

I'm curious about the START pin and synchronization functionality. Would our FPGA need to trigger a one-shot conversion and START signal every time a reading is taken? This might be annoying for our FPGA. 

Datasheet made us think yes, I'm curious if there's another recommended way to synchornize 2-4x of these without a START pulse needed every reading. 

Thanks!

-Cameron 

  • Hello Cameron,

    ADS127L21 is typically used in continuous conversion mode (START/STOP mode).  In this case, once the START pin is set high and held there, the ADS127L21 will continuously convert data and toggle the /DRDY pin at the data rate, with a falling edge on DRDY indicating when new conversion data are ready to be read by the host processor.

    Regarding your question, no, the FPGA only needs to send a single START rising edge to synchronize all ADCs when using START/STOP mode.

    In order to synchronize multiple ADS127L21's, all ADCs should use the same clock and a common START rising edge will then synchronize all ADCs.  For more details regarding synchronization, please take a look at this application note.

    https://www.ti.com/lit/pdf/sbaa520

    Regards,
    Keith Nicholas
    Precision ADC Applications