Other Parts Discussed in Thread: RCV420
Tool/software:
Hi folks!!
I have 3 questions regarding this AD converter:
1) In the spec it says that the mininum clock frequency is 16MHz. Is it possible to use Raspberry Pi 4 to conect it via SPI ?
2) Spec says that maximum voltage error is 4mV . I was thinking to use an analog multiplex to select one input for data channel and another one for zero voltage. After reading the zero voltageI would ajust the reading by subtracting the value from it . Is it a reasonable solution to correct the offset error?
3) Spec says that the maximum %FSR is 0.01. I use 5V as Vref , so the maximum error is 0,005v. So I'm planning to use the same multiplex and read this value and adjust all voltage readings. My question is: is it reasonable to do this way ?
Thanks!
Regards
Andre