This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Dear Madam or Sir,
Is it possible to get ADC3683EVM FPGA design project files for the AMD (Xilinx) FPGAs?
Thanks in advance!
Best Regards,
Zoran
Hello Zoran,
Apologies for the delayed reposnse. We typically do not give out the design files for our FPGA firmware, but we do provide a generic firmware for evaluation or custom firmware if you require anything more complicated than basic evaluation. Is there a particular mode that you would like to get working?
Best,
Luke Allen
Hi Luke,
Thanks for your support.
I’ll prepare the list of our point(s) of interest ASAP.
BR,
Zoran
Hi Luke,
I would like to ask you for the FPGA design (firmware) which could be used in the following ADC3683 mode:
- Resolution: 16 bits
- Sampling frequency: 65MHz
- Serial LVDS: two lanes
- Decimation: 4
I hope that these could be accomplished with ADC3683EVM plugged to Xilinx ZCU102.
Thanks in advance!
Best regards,
Zoran
Hi Luke,
Please take a look at my ADC3683 modes, down below:
- Resolution: 16 bits
- Sampling frequency: 65MHz
- Serial LVDS: two lanes
- Decimation: 4
I hope that these could be accomplished with ADC3683EVM plugged to Xilinx ZCU102.
Is it possible for you to provide such code for me?
Thanks in advance!
BR,
Zoran
Hi Zoran, we have taken this discussion into an email thread, so I am going to close this E2E post.
Best,
Luke Allen