Other Parts Discussed in Thread: ADS8364
Hello,
I am using the Analog to Digital Converter IC ADS8364 in my board.
A
sensor output is signal processed by an opamp and fed to the input
channel of AD8364 in single ended mode. (CHx negative connected to +2.5V)
At times, there are good probabilities that the input to the ADC may go beyond +5V and below 0V at CHx +.
I could see that the ADC input is having a voltage clamping scheme internally.
Please let me know if the ADC can withstand continuous voltages from +11V to -11V (opamp saturation voltage).
I tried clamping the ADC input with a Zener, but it has exponential
characteristics near breakdown region and is unfit for accurate
measurement purposes.
To limit the power dissipation in the
internal clamping diodes, I can connect a resistor in series to the
opamp output and ADC input.
If, by connecting a series resistor the ADC can tolerate +11V to -11V, please suggest the series resistor value.
Since the board is already fabricated, I am unable to connect those clamping rectifier diodes externally.
Thanks and Regards,
Mohmed Anees