Part Number: ADS1299
Tool/software:

Hello, I am doing board bring up for the above design and have noticed that the VCAP values are off. In addition I am having trouble communicating with the device. These are the measurements I have taken:
VCAP1 = 1.2V
VCAP2 = 2.5V
VCAP3 = 6.8V
VCAP4 = 0.3V
VREFP = 0.2V
VREFN = -2.5V
AVDD = 2.5V
AVSS = -2.5V
DVDD = 3.3V
If someone can verify my design and check if these voltage values normal that would be great.
Thank you!