DAC39RF10: Spurious : 8388.608MHz clock output from LMX2615 to DAC39RF10

Part Number: DAC39RF10
Other Parts Discussed in Thread: ADC12DJ3200

Tool/software:

We are using LMX2615 for DAC39RF10 and ADC12DJ3200.

LMX2615's Output clocks are 8388.608MHz for DAC and 2097.152MHz for ADC.

At low temperatures around 0 degrees Celsius, there is below issue.
Our board has the spurious about 35dBc at +-2.08MHz from fundamental frequency of DAC. Of course, if DAC output frequency is changed, the spurious occurs around +/- 2.08MHz at that changed frequency.

We have two similar boards with DAC39RF10, and only one of them generates the spurious at low temperature.

Also, We measured the 8388.608MHz between LMX2615 and DAC39RF10.
There are the spurious about -80dBm at +-2.08MHz from fundamental frequency(8388.608MHz)
We controlled the power down of DAC39RF10(controlled by SPI : DAC Register 0x0002 0x03), then the spurious between LMX2615 and DAC39RF10 has been eliminated.

We are digging the DAC's input clock buffer power(VDDCLK10), core clock power power(VDDCLK18) noise and also pull up matching circuit between LMX2615 and DAC39RF10 for the spurious issue debugging.

Do you have any clue for this issue?

please refer the below schematic.