Part Number: ADS7138
Other Parts Discussed in Thread: ADS7066
Tool/software:
Hi TI Team,
There are a few questions related to the 12-bit ADC converter (ADS7138):
-
How can we ensure that the ADC is set to either 12-bit or 16-bit mode? The documentation mentions that oversampling converts the 12-bit output to a 16-bit effective result, but is the core resolution still 12-bit only?
-
Though the ADS7138 is a 12-bit ADC, it seems to output 16-bit values after averaging. Can you explain how it achieves 16-bit results? This isn’t very clear from the datasheet.
-
The high threshold for alerts is specified as 0xFFF in the datasheet. If the averaged output is 16-bit, should the threshold be set to 0xFFFF? How does this work given the 12-bit core resolution?
-
What is the purpose of the OSR[2:0] bits in the OSR_CFG register?
- What is the maximum current that the ADS7138 can measure?
Thanks,
Manikanta