Part Number: ADC34J45
Tool/software:
Dear sirs,
I am working with ADC34J45 and I have a problem related to the phase noise with the digitized signal.
Configuration of ADC34J45 is shown as follows:
- Input frequency = 47.4 MHz -20dBm Without modulation
(-84dBc to 25KHz offset with BW=25KHz)

- Frequency clock: 158.4MHz LVDS Level about 0 dBm to the input of ADC
(85dBc adjacent channel to 25KHz offset (BW=25KHZ))

But the signal digitized by ADC is showing a high phase noise and very bad adjacent channels
Please, find below the digital signal analysed with MATLAB.

Zoom in 47.4MHz:

As you can check, phase noise is very bad in comparison with the phase noise of input signal and the clock signal.
I have checked the power supply increasing the DC filter to the input of low noise LDO which is used to supply +1.8AVDD to the ADC. I am using LDO from Texas TPS7A9101DSK.for 18AVDD.
Please, find attached a file with the samples of ADC, the values in the file are multiplied by 4 related to the output of ADC.
Finally, the inoput impedance of ADC is 200 ohms, and therefore the 0dBFS is about +4dBm.
Please, could you help me witth this issue?
Thanks in advance.
Best Regards,
Pedro