Part Number: UCD3138128
Other Parts Discussed in Thread: UCD3028
Tool/software:
Dear,
I got a problem on UCD3138128 when I used the FusionX0ToHext to convert the X0 file.
I could use the the FusionX0ToHext to convert the X0 file to Hex file on UCD3028/3138. But the Program Flash of UCD3138128 is 128K bytes.
After I checked the document 'ZHCA434.pdf', it seems that the size of the ROM flash is only up to 32K bytes. So how should I use 'FusionX0ToHext' to convert the X0 file of UCD3138128?