Part Number: ADC3664EVM
Other Parts Discussed in Thread: THS4541
Tool/software:
The ADC3664EVM supports both AC and DC coupled inputs, and the guide for it says "By default, the EVM is configured to receive external inputs for the sampling clock and analog input via AC coupled, transformer (balun) inputs."
What actually needs to be done to the EVM to switch the inputs to DC coupling, are there hardware changes required with depopulating and switching components or is it relatively easy?
The schematic seems to have a lot of DNP components on the input path relating to the coupling circuitry, are these DNP components included alongside the EVM or would we have to source them if DC coupling is needed?
Additionally, does the paired software HSDC Pro, have support for a DC coupled signal?
Thanks
Taylor