Tool/software:
To reduce the number of connection pins between the ADS125H02 and the CPU, /RESET (pin 7) and START (pin 8) are pulled up to DVDD.
In this case, when a power-on reset is performed by turning on the power, will the registers be initialized and AD conversion automatically start in continuous conversion mode (20 sps)?
Also, when changing the settings, is it okay to send a stop command to stop AD conversion, then set the registers and finally send a start command?