Part Number: ADS7052
Tool/software:
If we limit the current to the specified 10 mA and don't care about what happens to the data, can we occasionally
drive a bit of current into the positive analog input, specifically into the upper ESD diode,
without a latchup or other hazard?
Yes, this technically violates the abs max input voltage, but what will actually happen?