Part Number: AFE5832LP
Other Parts Discussed in Thread: AFE58JD32LP
Tool/software:
Hi,
Please tell me about the initialization of the AFE5832LP.
(1) What kind of malfunctions are expected to occur if the contents of section 10.4 of the datasheet are not performed?
(2) Are the following three registers the only ones related to "1. Write all bits marked 1 in all the register maps"?
・address 0x3 bit[4]
・address 0xD1 bit[2:0]
・address 0xD4 bit[0]
Regards,