Tool/software:
Hi Sir,
There's DAC43204 and CG5162 at the same I2C bus. Customer report that there's issue when they read CG5162's reg 0x20, there might have issue at its read byte: abnormal pull down happened at its bit 8 and only happened at reading 0x20. If they remove DAC43204, the issue is gone.
Normal waveform:
Issued waveform:
CG5162 has internal 4.7K pull up resistor, and cusomter add another 2K pull up resistor to 3.3V.
Do you have idea what's happened at the I2C communication at DAC43204? Any suggestion for checking the issue? Thanks for your kindly help.
Regards,
Gary Teng