Part Number: ADS1158
Tool/software:
Hi,
Sorry for the basic question, but I would like to know about the following question from a customer.
"Is the full-scale range when used in single-ended half that when used differentially?"

Looking at Table 7 in the datasheet, INPUT SIGNAL VIN = ADCINP - ADCINN
In the single-ended case, I think the input range is AINx - AINCOM. I think this is essentially a pseudo-differential input, is that correct?
For example, in the following setting
+VREF=2.5V, -VREF=0V
AINx = 0 to 2.5V
1. When AINCOM = 0, the output code is 0 to 0x7FFF
2. When AINCOM = +VREF/2, the output code is 0x8000 to 0x7FFF
Is this correct?
Best regards,
Hiroshi