This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8674: How to add the channel adress in Output Data

Part Number: ADS8674


Tool/software:

In our application, data is very rarely corrupted. Only on a few devices and less than once a day.

The ADS8674 is operated in MAN_Ch_n mode as described in the datasheet on page 46. The first 16 bits of the SDO data should be zero, but this is not the case. This may be due to EMI or mechanical connection problems. In this case we discard the data. To improve this sanity check, we would like to enable the addition of the channel address to the data by setting the SDO bits to 01 in the "Feature Select Register". But it is not clear to me where data bits 8-5 of table 13 are in the data stream. Do we need to continue clocking after the 32nd falling edge of the SCLK signal in Figure 102? In that case we could not keep the 500ksps right?

Thanks.