Part Number: ADS1258
Tool/software:
Hi
I am configuring the ADC in a certain way and I would like to be able to check the configuration I made.
For example, I set the MUXSG0 register as “10000001”, I want to see that configuration so I guess I should send a command for this with the register address, hoping that what I get back is that “10000001”....
I'm not sure if it's the Read Register Command = “010” having as Command “01000100”
What should I get as a response? how do I get those configuration values? simply "10000001"?
This for 1 specific register, but what about multiple register? whit MUL = '1'