Tool/software:
Hi,
I am working on DAC8775.
In the datasheet of DAC8775, under alarm section, there are some error in which open circuit is one of them.
When is the open circuit condition generated? Because there is no fault bit raised in status register and the Alarm pin doesn't go low.
DAC8775 is configured in current mode 4mA-20mA. count given was 0x7FFF.
I have attached the schematic below for your reference.
One more doubt, open short circuit condition is only for current mode or can it be used for voltage mode also?
Regards,
Nithin D