This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TX7364EVM: TX7364EVM

Part Number: TX7364EVM
Other Parts Discussed in Thread: TX7364

Tool/software:

hi,dear experts:

We purchased a TX7364EVM development board through the official website. Recently, we have encountered some problems during the debugging process. The specific descriptions are as follows:

We installed the TX7364 Demo software in accordance with the TX7364 EVM User's Guide. However, after I opened the Demo software, I couldn't find the option for the TX7364 chip in the scripts section.Also, we added the "devInit.py" file through the File subdirectory in the RUN drop-down menu, but it prompted that the hardware device could not be found.

We measured the various power supplies and clocks on the board, and confirmed that all the power supplies and the 250MHz clock were working properly. Moreover, the status of the LED indicator on the board was also normal.

The following is the screenshot of the interface:

I'm sincerely looking forward to the experts helping me solve this problem.

Thank you very much!