Other Parts Discussed in Thread: AMC7904EVM, USB2ANY
Tool/software:
Hi all,
I set up AMC7904EVM by User Guide.
1. Remove Jumper J10
2. Intall Jumper J11 to VCC-GND
3. Intall Jumper J9
4. Use power supply, provide -5V to EVM ( - connect black connector of EVM and + connect yellow connector of EVM)
USB2ANY connect EVM and get error message -44. what's problem by my setup?
then I test positive mode :
1. Remove J9
2. install J10
3. install J11 for GND-VSS
4. Use power supply, provide 5V to EVM ( + connect red connector of EVM and - connect black connector of EVM)
USB2ANY connect EVM and success to read register. but the local temp show 90C. Is it too high, right?
My probelm:
1. Disable LUT, to set DAC0/1/2/3OW_EN and write register 0x0000~0x00FF, the voltage always keep 4.78V
base on my test: Is the EVM board broken?