This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS9120: the difference of MSL(the same material)

Part Number: ADS9120


Tool/software:

Dear team,


Good day to you.


As for following materials, these MSLs are different regardress of the same materials.is it correct.

If yes, please tell us the reson. if no, could you tell me which is correct and revice the datasheet.

ADS9120IRGET : MSL 2
ADS9120IRGER : MSL 1


your confirmation would be highly appreciate.

Best Regards,

Kiroku

  • Hi Kiroku-san,

    Thanks for your question and patience as we were out of office for Thanksgiving holiday. Both materials should be MSL 1. I am seeing a recent PCN for ADS9120IRGET that reclassifies it from MSL 2 to MSL 1. The change may not be reflected on the webpage/datasheet yet. Both materials are tested at the same site, so both should be MSL 1.

    Hope that helps.

    Best regards,

    Samiha