Other Parts Discussed in Thread: THS4541
Tool/software:
I am writing to inquire about...
Based on your datasheet, we have implemented the recommended interface circuit with the following components:
- Operational Amplifier: "THS4131IDGKR"
- ADC: "ADS8422IBPFBT"
However, due to circuit constraints, the operational amplifier is powered with a ±5V supply. In this configuration, the input voltage to the ADC is limited by the output voltage swing of the operational amplifier, which does not meet the required ADC input range of ±4.095V or higher.
Could you kindly recommend a suitable rail-to-rail operational amplifier that meets the following criteria?
- Compatible for use as a front-end amplifier for the ADS8422IBPFBT
- Capable of achieving an output voltage range of ±4.095V or higher with a ±5V power supply
I appreciate your assistance and look forward to your recommendation.