Part Number: ADC3444
Tool/software:
I am using the ADC3444, and I would like to know the default register set configuration for this ADC.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADC3444
Tool/software:
I am using the ADC3444, and I would like to know the default register set configuration for this ADC.
Please see below
1. **Register 01h**: Default value is `00h` for all fields (DIS DITH CHA, DIS DITH CHB, DIS DITH CHC, DIS DITH CHD).
2. **Register 03h**: Default value is `00h` for ODD EVEN.
3. **Register 04h**: Default value is `00h` for FLIP WIRE.
4. **Register 05h**: Default value is `00h` for 1W-2W.
5. **Register 06h**: Default value is `00h` for TEST PATTERN EN and RESET.
6. **Register 07h**: Default value is `00h` for OVR ON LSB.
7. **Register 09h**: Default value is `00h` for ALIGN TEST PATTERN and DATA FORMAT.
8. **Register 0Ah**: Default value is `00h` for CHA TEST PATTERN and CHB TEST PATTERN.
9. **Register 0Bh**: Default value is `00h` for CHC TEST PATTERN and CHD TEST PATTERN.
10. **Register 13h**: Default value is `00h` for LOW SPEED ENABLE.
11. **Register 0Eh**: Default value is `00h` for CUSTOM PATTERN[13:6].
12. **Register 0Fh**: Default value is `00h` for CUSTOM PATTERN[5:0].
13. **Register 15h**: Default value is `00h` for CHA PDN, CHB PDN, CHC PDN, CHD PDN, STANDBY, GLOBAL PDN, CONFIG PDN PIN.
14. **Register 25h**: Default value is `00h` for LVDS SWING.
15. **Register 27h**: Default value is `00h` for CLK DIV.
16. **Register 11Dh**: Default value is `00h` for HIGH IF MODE0.
17. **Register 122h**: Default value is `00h` for DIS CHOP CHA.
18. **Register 134h**: Default value is `00h` for DIS DITH CHA.
19. **Register 139h**: Default value is `00h` for SP1 CHA.
20. **Register 21Dh**: Default value is `00h` for HIGH IF MODE1.
21. **Register 222h**: Default value is `00h` for DIS CHOP CHD.
22. **Register 234h**: Default value is `00h` for DIS DITH CHD.
23. **Register 239h**: Default value is `00h` for SP1 CHD.
24. **Register 308h**: Default value is `00h` for HIGH IF MODE<5:4>.
25. **Register 41Dh**: Default value is `00h` for HIGH IF MODE2.
26. **Register 422h**: Default value is `00h` for DIS CHOP CHB.
27. **Register 434h**: Default value is `00h` for DIS DITH CHB.
28. **Register 439h**: Default value is `00h` for SP1 CHB.
29. **Register 51Dh**: Default value is `00h` for HIGH IF MODE3.
30. **Register 522h**: Default value is `00h` for DIS CHOP CHC.
31. **Register 534h**: Default value is `00h` for DIS DITH CHC.
32. **Register 539h**: Default value is `00h` for SP1 CHC.
33. **Register 608h**: Default value is `00h` for HIGH IF MODE<7:6>.
34. **Register 70Ah**: Default value is `00h` for PDN SYSREF.
Regards,
Geoff
How we can configure, is there any existing values or any reference values, if i write that register what will be the output
Hi,
You can configure it through the SPI interface to the non-default values. Please see page 54 of the datasheet for more information.
https://www.ti.com/lit/ds/symlink/adc3444.pdf?ts=1733764631630&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FADC3444#page=54
Regards,
Geoff