This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS127L11: R94 of EVM schematic- what's this for?

Part Number: ADS127L11

Tool/software:

Fig. 2-1 of EVM schematic indicates R94=3.01 Ohm in series with AVDD1.  What is it's purpose and is it required?  I'm not seeing a description for it.

  • Hi Steve,

    The ADS127L11 has small internal bypass capacitors, in addition to the recommended external capacitors, and we have found that adding this external resistor results in lower noise and overall better performance of the ADC.  It is not necessary for functional operation of the device, but we always recommend including this resistor for improved noise performance.

    We do not specify this resistance, but any value in the range of 2Ohm to 4Ohm will work well, with 3Ohm as the typical value.

    Regards,
    Keith Nicholas
    Precision ADC Applications

  • Thanks much- would be great if you could update the datasheet, etc... with this info. 

    Thanks again!

    -Steve