This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4432: application queries

Part Number: AFE4432

Tool/software:

Hi Team,

Our customer is considering our AFE for PPG application. We promoted AFE4432 to them. Below are some application queries from customer. Could you please help to advise?


The product is a wearable wristband which is no need for medical certification. For AFE used in PPG, there are some application questions about the design of LEDs and PDs.

  1. As shown in TIs reference file sbat014 [ Product Overview : Photoplethysmography (PPG) With Integrated AFE for Optical Biosensing ], it can be seen using green LED for Heart Rate monitoring and using red & infrared(IR) LEDs for SpO2 monitoring.

    But in TIs another reference file sbaa556 [ Application Brief : Measuring Oxygen Saturation (SpO2) on Wearables ], it notes that A typical SpO2 system can use a green LED in addition to red and infrared (IR) LEDs.

    Can we use either “green LEDs + PDs” or “red & infrared LEDs + PDs” for Heart Rate and SpO2 measurement ? Strengths and weaknesses?
  2. AFE IC use multiple external LEDs and PDs to mitigate effects such as ambient light and motion artifacts,  does it ?
    For example, AFE4432 support up to 4 LEDs & 3 PDs, Can we reduce the quantity of LEDs or PDs due to the limitation of layout space or product ID?
    For Heart Rate measurement : the minimum quantity of LEDs and PDs ?
    For Heart Rate & SpO2 measurement : the minimum quantity of LEDs and PDs ?

Please help to confirm above questions. If you can share some relational reference file ,It would be better.

Thanks a lot !


Best regards,

Terry