Tool/software:
We are using DAC82001 for high accurcy voltage output. but we found strange jumps when testing.
Out design parameters are following:
Vref = 1.024V
DAC output data from 0 to 255, then 255 to 0, total 256 steps.each step 40ms.
Can someone give any suggestion about this observation? I guess it is related with the switch from such as b'011111 to b'100000, but have no evidence.
Thanks.