Other Parts Discussed in Thread: TVP5158
Hi,
We are using TVP5158 in one of our design. We have prototype board with us and conducted Radiated emission test on our design.
Test Observations:
System is failing at 81MHz frequency. We have 2 crystal and one oscillator of 27MHz. We have disconnected all the 27MHz source except the one connected to TVP5158. We observed that emission at 81MHz remains at the same level.
Design Details
1) We have used ABM10-27.000MHZ-E20-T(Abracon corporation) for TVP5158 frequency input
2) We have separate ground VSSA and VSS. Both VSSA (Analog Ground) and VSS(Digital Ground) are shorted with Ferrite bead (BLM15AX601SN1D) which has 600E impedance at 100MHz.
Queries:
1) Is it necessary to connect XTAL_REF(pin 100) of TVP5158 through 0E resistor to VSSA? TVP5158 datasheet says that pin 100 is internally connected to analog ground. EMI results shows improvement after disconnecting pin 100 from analog ground
2) When we remove ferrite bead between analog ground and digital ground, we see improvement in EMI results. Please suggest best way to isolate Analog and digital ground
Please also let us know any additional measure in layout apart from the layout guidelines for TVP5158.
Best Regards,
Swapnil Kanani