This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
From this table in the datasheet, if Vref is 2.5V, I calculated that the LSB should be 2.5 / (2^23 - 1) = 0.298 uV
Can anyone confirm if this is correct?
Hello Charles,
Yes, you are correct. Each ideal code step, or LSB size is 0.298uV. Note that in most cases, this is much lower than the noise floor, unless you do additional digital filtering on the data in your processor.
Regards,
Keith Nicholas
Precision ADC Applications