Tool/software:
Hi,
Our design maximum height is 1.4mm.
We found SOT235 package maximum is 1.45mm, but we meansure sample on hard all about ~1.1mm.
May I know why this tolerance is big?(and it seem same SOT23 package with DDCR? but DDCR only 1.1mm max.)
If we choosing SOT23 (6) can replace directly? PG pin can let it floating, right?
I found SOT23 (6) heigh maximum only 1.1mm.

Thanks!
Jeff