Part Number: ADC32RF45
Other Parts Discussed in Thread: LMK04828
Tool/software:
I am using ADC32RF45 with JESD204B subclass 1 and I/F with FPGA. When I input one pulse of SYSERF from PLL to FPGA and ADC for linking, a disparity error is detected on FPGA side and I cannot link properly.Any suggestions for a solution to this problem would be appreciated.


As a precondition, we would like to make sure that the sample position from which the ADC data is acquired does not shift even if the JESD link is redone by turning the power on and off again.
Environment:
* Use LMK04828 for PLL
* Use XILINX JESD204 v7.2 IP on FPGA
* Input 3GHz clock to CLKIN1 of LMK04828
Remarks:
* The same phenomenon occurs on evaluation board (ADC32RF45EVM)
* If SYSREF_MUX of LMK04828 is not changed to Normal SYNC but left as SYSREF continuous, it links normally after several SYSREFs.
Attached file contents:
1. configuration file of PLL used on the evaluation boardLMK04828.cfg
2. configuration file of ADC used on the evaluation boardADC32RF45.cfg