This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8681: ADS8681 Setup compete silent

Part Number: ADS8681

Tool/software:

Hello everyone,
I am looking for the silent installation parameters for the setup ADS8681_EVM.exe. It should install ADS8681, National Instruments software and the Windows driver package - Tesys Instruments silent.
Can anyone help me with this?
Thank you

  • Hi Marco,

    Welcome to the TI E2E Forums!

    I believe running "Setup_ADS8681_EVM.exe --mode unattended" will get you part way there, but there may still be some pop-up notifications for the USB Driver and NI Software since those are embedded installers that likely require additional parameters to run in silent mode.

    Would you be so kind to provide additional details about why this installation mode is preferred or needed for the GUI?

    Thanks and best regards,
    Chris

  • Hello Chris,

    the software should be installed via a deployment tool on several computers on which the users are not administrators. Therefore the complete installation should be executed in silent mode

    Greetings Marco