Part Number: DAC3482
Tool/software:
IF I AM USING ONLY BPSK MODULATION (NEED ONLY ONE BIT) CAN I CONNECT ONLY THE MSB BIT AND LEAVE ALL THE OTHERS “NC” OR DO I HAVE TO CONNECT TO ALL 8/16 DIFF PAIRS DEPENDING ON BYTE/WORD MODE
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC3482
Tool/software:
IF I AM USING ONLY BPSK MODULATION (NEED ONLY ONE BIT) CAN I CONNECT ONLY THE MSB BIT AND LEAVE ALL THE OTHERS “NC” OR DO I HAVE TO CONNECT TO ALL 8/16 DIFF PAIRS DEPENDING ON BYTE/WORD MODE
Ohad,
This depends on the byte/word mode. In byte mode, you will have to connect all pairs. (MSB is shared with bit 7 in byte mode since it is a single line for both MSB and bit 7, see datasheet diagram for byte wide mode).
In word mode, you can connect MSB to logic HI (with respect to LVDS threshold), and other pairs to logic LOW (with respect to LVDS threshold). Keep in mind that you would have to use offset binary mode in this fashion. TI also cannot ensure that the customer can achieve the performance needed with respect to the datasheet.
-Kang