Other Parts Discussed in Thread: ADS7038-Q1,
Tool/software:
Hi
Could you provide the driver demo code for ADS7039 auto-sequence mode?
I can only find the manual mode demo code.
thanks!
Tool/software:
Hi
Could you provide the driver demo code for ADS7039 auto-sequence mode?
I can only find the manual mode demo code.
thanks!
Hi Yan,
Unfortunately we don't have anything at this moment to showcase the auto-sequence mode. Is there anything specific you would like to accomplish with it? Maybe I can help you in coming up with a command sequence for it.
Regards,
Joel
Hi Joel
thanks for your reply
my sequence of commands:
1. Reset
2. Channel ID append enable
3. choose auto-sequence mode
4. Channels 0, 1 and 6 activated for auto-sequencing
5. Start Sequencer
The SPI rate is 2M, transmit and receive FIFO are enable.
After these configuration steps , I can not receive the sampling result. Is there any missing step? Do I need to configure the sampling rate by OSC_SEL and CLK_DIV?
In auto-sequence mode , set SEQ_START to 1 for one time and it will trigger the continuous sampling without the rising edge of CS yes?
Hi Yan,
Can you clarify if you are asking about ADS7038-Q1 or ADS7039-Q1? From your description, it seems like you are referring to ADS7038-Q1. Am I correct? If so, I will delete this thread and ask for you to post a new thread under the relevant device.
Regards,
Joel