Part Number: ADC3642
Tool/software:
Hello,
I try to configure the ADC3642 to work with the following configuration but I encounter some issues ...
- Output mode DDR
- Single ended clock
- 14bit data
- Sample rate 10MS/s
- SPI SCK : ~2.5MHz
Please find below the commands that I send to the chip through SPI:
- Reg 0x000 - Value : 0x01
- Wait for ~1.6ms
- Reg 0x007 - Value : 0xA9
- Reg 0x013 - Value : 0x01
- Wait for ~1.6ms
- Reg 0x013 - Value : 0x00
- Reg 0x00A - Value : 0x23
- Reg 0x00B - Value : 0x46
- Reg 0x00C - Value : 0xF0
- Reg 0x00E - Value : 0x09
- Reg 0x011 - Value : 0x35
- Reg 0x01B - Value : 0x90
- Reg 0x01F - Value : 0x90
- Reg 0x08F - Value : 0x02
- Reg 0x092 - Value : 0x02
- Reg 0x014 - Value : 0x10
- Reg 0x015 - Value : 0x00
- Reg 0x016 - Value : 0x00
NB: I have also tried to set the value 0x00 on register 0x000
I dont' have any clock in output on pin 25 (DCLK) and I don't understand why.
Is there something wrong with my configuration ?
I add below some pictures of the SPI signals I send.



Thanks in advance for your help and merry christmas !
Regards,
K. TOUTAIN