Hi,
I'm usingTVP7002EVM, Can I use TVP7002EVM to convert VGA to HDTV? For example,the input of TVP7002's is 1280x1024@60 and
the output of THS8200' is 1080i@50.
Thanks in advance!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm usingTVP7002EVM, Can I use TVP7002EVM to convert VGA to HDTV? For example,the input of TVP7002's is 1280x1024@60 and
the output of THS8200' is 1080i@50.
Thanks in advance!
You will not be able to change formats and resoutions using just the TVP7002 EVM. You would a graphics processors with frame buffer, scaling capabilites, and interlace/deinterlacer for this.