Part Number: ADS5409
Other Parts Discussed in Thread: ADS5402EVM, , ADC12DL3200, LMK04832, LMK04828, LMK61E08
Tool/software:
Hi Team,
1) In the below image of ADS5402EVM, Pin number P10, N10 are used as trigger pin function. But in datasheet it mentioned as do not connect pin. What should we consider this pin function in our design?


2) How to give Clock input for ADS5409
We referred some other ADC part number - ADC12DL3200, clock signal from LMK04832 is given to both FPGA and ADC.
Do we also need to implement the same for ADS5409 and FPGA.

3) Since ADC5409 sampling rate is 900Msps. We selected this clock oscillator which supports LVDS 900MHz. Shall we proceed with this part number or suggest any other part number supports for ADS5409.