Part Number: ADS131M06
Tool/software:
I want to use the built-in oscillator is the ADS131M06 with a standard 8.192 MHz quartz crystal. However, I can't find a proper application, neither in the datasheet or anywhere else. Even the evaluation board uses an external oscillator.
Is there a list of applicable quartz crystals available, or, alternatively, a proper specification for the crystal, including ESR, load cap, etc.?
In other applications it is mandatory to use small capacitors to ground, in order to adjust for the load capaitance. Is this necessary for the ADS131 or even couner-productive? What is the built-in pin capacitance of XTAL1/XTAL2 anyway?
Many thanks,
Ralf