Part Number: ADS8329
Tool/software:
Hello forum members!
I am troubled by the phenomenon that the AD conversion result is offset in the + direction.
The following is an explanation of the situation.
The ADS8329 is operating in auto trigger mode.
3.3V is supplied to +VA and +VBD.
REF- is connected to GND and 3.0V is supplied to REF+.
Other peripheral circuits are set according to the recommended circuits (constants) in the data sheet.
Checking the AD conversion data obtained by the command “Dh”, a deviation equivalent to about 0.2V is generated.
For example, even if 0V is set between the +IN and -IN pins, the AD conversion value read out is “388”.
Is there any possible cause for the offset of the AD conversion value?
Please let us know if there are any items to check.