Other Parts Discussed in Thread: LM7705, LM27761
Tool/software:
Hi,
We use the DAC8760 in our project and there are some issue for our deisng:
1. When using DAC8760 to simulate output voltages of 0~5V and 0~10V, it is not possible to output voltages below 0.064V. how to solve this issue?
2. When simulating the maximum output voltage and the maximum output voltage is 5V+0.06V, but not 5V. Is this issue related to the one mentioned above item#1?
3. Below is our schematic diagram for your evaluation, thanks.