Tool/software:
The full part number is TPS7H4002HKH/EM. Have discoloration on their welds.
what the cause of discoloration could be and if it is safe to use as is?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
The full part number is TPS7H4002HKH/EM. Have discoloration on their welds.
what the cause of discoloration could be and if it is safe to use as is?

Hi Robert,
I just replied to your other post as well, but I will also put the same information here.
There are two general reasons why discoloration can happen with units:
1. Oxidation
2. Salt in the atmosphere.
In either case, TI has done testing on discolored units and they have passed lead-fatigue/solderability tests.
Our stance is that discolored units do not impact package integrity, lead integrity, or solderability degradation.
Thanks,
Sarah