Part Number: ADS127L21
Other Parts Discussed in Thread: OPA2192, OPA2325, OPA2328
Tool/software:
Hi TI Team
I have two questions.
1. We plan to use the ADC in a safety PLC certified according to the IEC 61508 standard. We need to achieve SIL2 with a proof test interval of 20 years. Is this possible with just using a single ADS127L21 and the build in safety features (CRCs, STATUS1 & STATUS2) and by checking the DRDY signal frequency? Or is mandatory to have some sort of control method (second ADC, reference measurement)?
2. Is the OPA2192 a suitable driver for the inputs?
Regards Theo